This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

About Output inpedance of SN74LVC04A

Guru 19645 points
Other Parts Discussed in Thread: SN74LV04A, SN74LVC04A

Please let me know about LVCMOS output inpedance(Zo) of SN74LV04A.

【Background and condition】

・SN74LVC04A using for clock driver(50MHz)

・Inpedance matching of this pattern is 40~50Ω

・Output side is connected 22Ω-danping for waveform shaping.

⇒Customer want to know these circuit is maching or not.

Best regards,

Satoshi

  • Hi Satoshi-san,

    A 50 ohm load on this part will exceed the part's drive capability (max of ~12mA at 3.8-V Voh)

    My math:

    Vo / Rload = Imax (maximum output current required)

    5V / 50ohm = 100mA

    If Voh were to dip to 3.8V (lowest value listed on datasheet),

    3.8V / 50ohm = 76mA

    Since the part can only output ~12mA max, I would recommend looking into a different solution.

    Can you tell me more about your application?

  • Correction*

    The output will have to source half of what I listed, but 50mA and 38mA are still much higher than what the device can handle.