Other Parts Discussed in Thread: PCF8575, PCF8575C
Good morning
I have a problem driving output of PCF8575 . I have all output disconnected (they are floating)
now on I2C I only send this command
START I2C
0x40 --- write at address 0x40 ------> ACK 0 level from PCF on ninth bit
oxFF --- all output on ----->> ACK ACK 0 level from PCF on ninth bit
oxFF --- all output on ----->> ACK ACK 0 level from PCF on ninth bit
STOP I2C
All outputs at last ACK go at level 1 3,3V but after STOP condition they return to 0V like a discharging capacitor
Why this behaviour?
must I send a 0x00 command before send write command?
Thank you very much