Hello,
In 8.3.4 on page 13 of SN74LVCH8T245 datasheet (SCES637B, Aug 2005, Revised Feb 2016), it states that it supports 3.3V to 5V conversion with max frequency at 200MHz.
However, in Fig 16 on page 16 of Understanding Advanced Bus-Interface Products, SCAA029 May 1996, it states that the functional frequency using standard load specified in datasheet for LVC device is 125 MHz.
So, which one is correct? Could SN74LVCH8T245 support transfer rate at 200MHz?
Best regards,
Mark