I am thinking about using this switch SN74LVC2G66 to switch some GPIO interfaces in order to prevent backpowering my device through the GPIO ports even when there is no power supply present to the device.
But, the datasheet indicates there is some ESD protection, but the diode situation is not indicated in the schematic diagram. Are the protection diodes only to GND? Or do they also go to SN74LVC2G66's Vcc? Obviously if there are ESD diodes to the switch's Vcc then it won't prevent backpowering at all.
Vipa