Other Parts Discussed in Thread: SN74LVC8T245, TXB0108, SN74AVC8T245
We have a board where TXB108 level translator is seen driving a high density 16-wire ribbon cable of about 3ft. This cable is routed along with host of other flat cables.
The receiving side has SN74LVCxxx series driving similar flat cable.
During system integration, turns out that the cable position affects proper functioning of the interconnected boards ...some signals seem to be corrupting logic levels. By separating the cables & placing along a specific path inside the chassis seems to make the system functional.
So it is a case of such chips not being able to drive cables we have.
We do not have high speed signal at all in any path. Max may be 1MegHz clock.
There is really no level translation going on. All sides are 3.3V referenced to DGND on either side.
One way to debug would have been to remove/replace with a chip capable of driving such lengths. But I have not found any.
If I made a tiny pcb as an interposer board, which chip would be most optimum to use in this situation?
We clearly want the cabling to be insensitive to where/how it is routed. Since I suspect drive capability itself, adding shielding here would be making the situation even worse.
Looking for a clean solution.
thnx
robin