This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Difference between level translator and Line Driver

Other Parts Discussed in Thread: TMS320F28069

Hi,

Ref: TI  product lines:

1. Voltage Level Translation

2. Buffer/Driver/Transceiver

What is the exact difference between the two product lines. It seems one can voltage traslate from a Buffer/Driver/Transceiver also. Kindly suggest when to use a Buffer/Driver/ Transceiver and when to use level translator product.

I have 7 PWM outputs from TMS320f28069 (3.3V Logic), want to drive IGBT Driver (which requires 5V Logic). Which product line should I go with, to select an interface IC??

Thanking you,

Siddharth Gupta