Hi,
looking at the data sheet (REVISED JUNE 2015) , I'm missing the max rise time specification.
Need this info for a big project, can someone help out here please?
Thanks a lot
Steffen
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
looking at the data sheet (REVISED JUNE 2015) , I'm missing the max rise time specification.
Need this info for a big project, can someone help out here please?
Thanks a lot
Steffen
Thank you.
Is that really a limit like a max rating or just a recommended operating?
What else than the increase current consumption is expected when violating 20ns/V at 1.8V?
My problem: The rising CLR_N (tr=30µs) doesn't trigger the output, whereas tr=30ns does it.
I would expect an output trigger at any transition time. Are there other reasons preventing an output trigger?
regards Steffen
The recommended operating conditions guarantee that the device works.
The absolute maximum ratings guarantee that the device does not go up in smoke immediately.
A too-slow rise time typically results in oscillations in the output (see Implications of Slow or Floating CMOS Inputs (SCBA004) for details). In the case of a clock signal, these oscillations might be too fast for the rest of the circuit, so the behaviour of the device will be entirely unpredictable.