This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Using TXS102 in a portable device

Hi everyone,

I've got a problem on a portable device. I've got an IC with and an i2c bus. This device is feed with a Li-Ion battery, so the level voltage is from 2.75V to 4.2V and I have to communicate this IC with a microprocessor feed with 3.3V. So according to the TXS102 datasheet:

VCCB = VBAT

VCCA = 3.3V

When the battery has a voltage from 3.3V to 4.2V there isn't any problem but when the battery is from 3.3V to 2.75V and according to the datasheet of the TXS102 VCCB has to be >= VCCA (3.3V). So I've got a problem.

Does anyone how to solve this problem?

Best regards.