Other Parts Discussed in Thread: CD4046B
I do not have much experience with PLLs; but I do have a requirement that I need help with.
Can the 74HCD4046 (CD4046 in general) have the ability to make a PLL that can function from 10kHz to 1 MHz and speed up the output to be 40kHz to 4MHz?
I have tried using the CD4046 to test out a PLL, but the VCO was only able to output 1.8kHz at 5Vcc.
The limitations I have here is that it needs to be TTL up to 5V.
I will be needing this to use for a Quadrature Demodulator.