This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TXS0108E for translating from 0÷3.3V to 0÷5V open drain

Other Parts Discussed in Thread: TXS0108E

Hello,

I have a customer trying to translate from 0÷3.3V to 0÷5V open drain using the TXS0108E.

When they apply 3.3V then the translation to 5V is correct.

But when they apply 0V then translation on TTL side is ~1.3V.

They're looking for a solution to translate the 0V of the 0÷5V open drain to 0V (Instead of 1.3V).

Can this be done with the TXS0108E ?

Should they use different part ?

BR,


Nir.