Other Parts Discussed in Thread: TXB0104-Q1
Hi Team,
I hav e some questions related to OE Pin.
As I know, TXB0104-Q1 can be controlled by the external signal from MCU and connecting from 5V bias to enable IC.
When 5V bias to OE pin is connected to enable, do I have to connect pull-up resistor? If yes, which resistance value is recommended?
And what do I have to caution to use the bias 5V?
Thanks,
WS