Hi,
I have a question about Vcca and Vccb tolerance of TXS0104E.
Customer now is using 3.3V for both Vcca and Vccb, but these two 3.3V are generated by two VRs.
There are 1% tolerance on the 3.3V, which means the real operation may have Vcca=3.33V(3.3*1.01) higher than Vccb=3.267V(3.3*0.99).
Is it a concern on this case? And customer would like to know the max tolerance of Vcca > Vccb.
Thank you.
Best regards, Cage.