This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LV541ATRGYR Thermal Questions



Questions about the SN74LV541ATRGYR:

1) The table at the end of the datasheet suggests the operating temperature range for this package is up to 85C.  Is this the max ambient air temp?

2) The theta_ja for this package looks the best of all the available packages.  What limits this to 85C?

3) Is there a theta_jb and theta_jc available? We have mechanical engineers that help analyze thermal considerations.

4)  How can the temp rise be calculated?  The datasheet provides theta_ja numbers but there doesn't appear to be any max power dissipation spec to multiply by the theta-ja.

I would like to use these components where a board temperature can be in 94 deg C to 100 deg C range, and would like to know if this is possible.

Thanks, David

---------------------------------
David Hildebrand
Analog Field Applications
South Region
Texas Instruments, Inc.
Office:  214-479-0917
Cell:       972-841-6499
david.hildebrand@ti.com
---------------------------------