Other Parts Discussed in Thread: TXB0304, SN74AVC4T245, SN74AVC4T774
Hi team,
My customer is using TXB0304 in an application that FPGA<->TXB0304<-->TXB0304<-->FPGA.
Between FPGA and TXB0304 is 1.8V logic and between TXB0304 & TXB0304 is 3.3V logic.
Customer wants to achieve 100Mbps data rate in such application. But I could only find in datasheet that TXB0304 capacitance is ~34pF and TXB0304 could achieve 130Mbps when CL is 30pF and Vcc>=1.8V.
Could you help to confirm whether in such customer application, 100Mbps could be achieved or not?
Thank you!