This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Maximum REXT and CEXT values that can be used with 74LVC1G123 ?



We want to use 74LVC1G123 to derive a High going pulse of width close to ten seconds.

Going by the Calculations in the datasheet , there is no limit provided on the values of REXT and CEXT . Per my requirement i need to use either

1. 1M ohm resistor with a 10uF capacitor OR

2. 10M ohm resistor with a 1uF capacitor

My question is that whether these kind of REXT/CEXT values can be used with 74LVC1G123 and in fact whether it is possible to acheive this value of pulse width using 74LVC1G123


Regards

Jitender