Hi ,
I am trying to run 4 Stepper Motors from a Micro Controller, Instead of using uC's GPIOs ,
I am thinking of using 4-16 Demultiplexer, One possible way is to use 4* 1-4 Demux with shorted address pins.
Is there any IC which can do this ? Or How do I achieve this design?
Another question is as I am driving the Motors using Motor driver [ I need to use 4 Motor Drivers , which I am trying to reduce by putting the Motor Driver before the Demux circuit ]. But Motor Driver like L293D or DRV8835 puts up a max 1A current , Is there any Demux which can handle that much Input Current and Heat Dissipation. Suggestion of alternative design is welcome.
Thanks in Advance
Naveen G