This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74ABT574A Maximum Ground Current



Hello,

The 74ABT574A specifies a maximum current per output pin of IOH=-32mA, IOL=64mA.  Is there a maximum current limit for the power and ground pins with all IO pins sourcing 32mA or sinking 64mA?

Thanks,

Keith N.
AFA OH/wPA

  • Hi Keith ,

    Within the recommended operating conditions of IOH / IOL , the Vcc/gnd pins can withstand the continuous current through it. Please be aware to take into account the Icc (and/or delta Icc) when inputs are not at the rails .
    I do not see a spec on the datasheet on the abs max continuous current though Vcc/gnd .