Hello,
We would like to use SN74AVC1T45DCKR in a scenario where VCCA =3.3V and VCCB = 3.3V. I have seen voltage translators where VCCA cannot be equal to VCCB. However in the case of SN74AVC1T45DCKR, it was not very clear from the datasheet whether VCCA can be equal to VCCB ( VCCA=VCCB=3.3V in our case). Could anyone please clarify regarding this? We have used the SN74AVC1T45DCKR for level translation in other sections of the design and would prefer to use the same device for isolation purpose instead of adding one more line item on the BoM. Therefore, this question.
Best Regards
SN