Hi Team,
I am using the CD40107B NAND Gate in my application in the following manner:
Can you please help answer the following questions:
1. This is not used in the typical open drain configuration, where the output is pulled-up using a resistor and then applied to a load as follows:
Is it ok that the load is part of the pull-up? What are the risks associated with this implementation?
In my implementation, I can use the FET inside the NAND gate to turn on and off my load, but since my load is part of the pull up I am not sure what consequences could result.
2. In the datasheet, there is a graph that I am struggling to understand:
If the output is "low" as it says in the caption, why is the drain-to-source voltage (Vds) at such large voltages?
I am assuming this graph is referring to the following FET:
In my application, Vss is tied to ground, so a Vds of 5V, 10V, or 15V does not seem like a "low" to me..
Thank you for your help here.
Jared