This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TXS0102 pull up resistor problem

Other Parts Discussed in Thread: TXS0102, SN74AVC2T245, SN74AVC2T45, SN74AVCH2T45, SN74AVC2T244, TXB0101

                I am account analog FAE of Suzhou IVO who’s the China leading panel maker customer. Now, we have DIN TXS0102 in their notebook panel for open drain level translator.

               As we known, the internal pull up resistor is 10k, when the input signal is floating, the voltage of point 1 is 3.3V*(1k/(1k+10k))=0.3V which is larger than VIL (max=0.15V), so the output status is unknown at this time. While, my customer requires the output voltage is low during the input is floating.

               I also checked the other type level translator (SN74AVC2T244, SN74AVC2T245, SN74AVC2T45, SN74AVCH2T45, etc.), but the datasheet doesn’t show the specific data regarding the pull up or pull down resistor.

               Could you give any suggestions regarding this requirement (the output is low when input is floating.)?

              

 Thank you very much.