This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LVCC3245A VOH and VOL

Guru 16770 points


Hi

Do you have value of VOHA, VOHB, VOLA and VOLB with the test condition of IOH=-100uA, IOL=100uA at VCCA=2.7V, VCCB=4.5V?

Could you confirm ti?

Bestregards

  • hi na na ,

    The datasheet conditions for the 100uA load suggests that the Voh is Vccx - 0.1V and vol is 0.1V . going by that :
    Voha = 2.6V
    Vohb=4.4V
    Vola=0.1V
    Volb=0.1V

    This would be my estimate on the voh vol although I do not have char data for the specific condition.