I apologize for the probably unnecessary question
For a motor control project I'm planning to purchase the TMS320C2000 Experimenter Kit among others. In the TMS320C2000 Experimenter Kit Overview (sprufr5f) document, I read the statement
-5.0-V supply for prototyping area
-3.3-V supply for prototyping area
Despite the F28335 being a 3.3V logic level MCU, are the GPIOs transformed to 5V for the 5V prototyping area. I can imagine that this is probably not the case, but without the board schematics this is something I cannot answer definitely on my own. Would the SN74LVC2G07 be a solution for, say, a pwm output or geartooth hall-effect sensor?
Thank you so much for your time