This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

about the skew between SN74AVCH4T245RSVR each channel

hi dear supporting team,

do you have the skew data between channels of SN74AVCH4T245RSVR? 

customer is using 3.3V VCCA and 1.8V VCCB,  they use both A to B and B to A directions.  because there is only min&max delay in the d/s, they want to know:

1.  the skew data btw each channel on same chip.  (better to provide min, typ, max skew number)

2.  for the same chip, will the skew & delay number change during operation?  or will it change with different time power up?