This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74AUP1G17 Vt+ and Vt-



Hi

I have checked some post on the E2E for this question.  However I do not understand exactly meanings of Vt+ and Vt-.

Vt+ means that the input range for high output. (the output is high level when the input voltage higher than the Vt+ (1.88 ~ 2.29V @Vcc=3V) 

Vt- means that the input range for low output. (the output is low level when the input voltage lower than the Vt- (0.88~1.24V@3V)

Is my understanding correct?

Regards,

Koji Hamamoto