This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74AHC123A Tw minimum value

Other Parts Discussed in Thread: SN74AHC123A, SN74LVC1G123

Hi support team

My customer  is considering to use SN74AHC123A  for one_shot pulse generator.

I was received an inquiry about tw minimum value from them.

Could you provide the data of minimum value of tw under these conditions as below?

(Condition No.1)

TA = -40℃ to 85℃

Vcc = 3.3V±0.3V

CL = 50pF

CEXT = 28pF

REXT = 2kohm

(Condition No.2)

TA = 25℃

Vcc = 3.3V±0.3V

CL = 50pF

CEXT = 28pF

REXT = 2kohm

Best regards.

  

  • Higa ,

    unfortunately , we don't have the min listed on the datasheet or the char data hence I cannot guarantee the min .
    I would expect the min to be close to 50-70ns.

    would you consider using sn74LVC1G123 which has the min and max listed for the condition ?