This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

The rating of TXB0106

Other Parts Discussed in Thread: TXB0106-Q1

The operating free-air temperature range of TXB0106-Q1 is –40°C to 85°C, and its rating is Automative. Why?

In my original oponion, the difference between Industive and Automative is Temperature, and the Automative rating should be –40°C to 125°C.

So why is TXB0106-Q1 Automative?

Many thanks.

  • Hello Luffy,

    There are different grades for automotive qualification. AEC-Q100 has following Automotive Grades:

    Grade 0 (or A): -40°C to +150°C ambient operating temperature range

    Grade 1 (or Q): -40°C to +125°C ambient operating temperature range

    Grade 2 (or T): -40°C to +105°C ambient operating temperature range

    Grade 3 (or I): -40°C to +85°C ambient operating temperature range

    Grade 4 (or C): -40°C to +70°C ambient operating temperature range