Hello,Sir
We have a cascade SN74LV165ARGYR design is eigth-74LV165A network constructed from a series of SN74LV165ARGYR. In our circuit, CLK INH is always pull 1K resistor to ground. We don’t implemented CLK INH feature. And VCC 3.3V and CLK is 2.667MHz.
When parallel inputs are static, we got SN74LV165ARGYR output (QH) wrong value question from the signal waveform and LA analysis result, but it only happened on the 8th one that 8th QH (=7th SER) series value became to “7C” from “6C” random and the issue may not happen continued. But add 8PF capacitor or Active probe touch on SN74LV165ARGYR Clock source, the issue will not happen again.
Attached are the circuit/routing topology, signal waveform and LA analysis.
In the normal and abnormal SGPI waveforms, 7th 74LV165 (/LD, CLK, SER) and data in (“E”, pin3) is on the 8th one. You can see SER of 7th 74LV165 (= 8th QH output) become 7C value when the parallel data in (“E”, pin3) on the 8th one is static.
Whatever normal/abnormal waveform, we also saw 8th QH start data output series data when /LD is still low level; QH output data should on the 1st CLK rising edge after /LD is high level.
Please kindly check the question and review the design.