Other Parts Discussed in Thread: TXS0101
Hello,
I'm using the TXS0101 in a level translation application configured as such:
VCCA = 1.8V
VCCB = 2.5V
OE = Connected to VCCA via a 10K pullup resistor
There is the possibility of VCCA being powered while VCCB is at 0V for prolonged periods of time.
Some questions:
1. The datasheet suggests that during powerup, VCCA can be greater than VCCB. Is there a time restriction on this requirement?
2. The datasheet also suggests that OE must remain low until VCCA and VCCB fully ramp. This is not the case in our circuit. Will this cause damage to the device?
3. When operating in this condition, are there any negative side effeects if the I/O on VCCB is driven to 2.5V, without applying VCCB?
Don