Other Parts Discussed in Thread: TXB0104
Hi,
In the datasheet of TXB0104 the maximum capacitive load at the output is mentioned as 70pF.
How can this be computed in mA when the IO voltage is 1.8V ?
Regards,
Bhavya
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: TXB0104
Hi,
In the datasheet of TXB0104 the maximum capacitive load at the output is mentioned as 70pF.
How can this be computed in mA when the IO voltage is 1.8V ?
Regards,
Bhavya
This limit is not directly caused by insufficient drive strength; section 8.3.3 says:
With very heavy capacitive loads, the one-shot can time-out before the signal is driven fully to the positive rail.
The VOH/VOL specifications have test conditions of 20 µA; this shows that this device is not designed to drive heavy loads in the steady state.
The drive strength of the one-short circuit is higher; it's designed to be able to fully charge the 70 pF load before the timeout expires. However, that current cannot be computed without knowing the timeout value.