Other Parts Discussed in Thread: TXB0304
Hi dear supporting team,
my customer met one issue on TXB0304, they are using it for BI-Direction level shifting btw CPU and TF card. CPU side is 1.8V (left side), and TF side is 3.3v(right side), they pull it up through a 20K resistor. (I asked them change to higher, they tried 80k, the issue is the same)
The issue is : when left side SD_CMD is 0V, right side H_SD_CMD is also 0V.
now if they pull the TF card, and in the mean time, they reset the left side CPU, when it is reset, SD_CMD should be high impedance. while now H_SD_CMD is still low level.
since currently both side has no driver, only right side has pulling up, the right side H_SD_CMD should be high, why it keeps low? could you help explain?
and I heard TXB0304 is not suitable for TF kind of applicaiton, is it right?
the sch is as below: