This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LVC1G123: SN74LVC1G123 minimum retrigger time calculation

Part Number: SN74LVC1G123

hi

For the "minimum retrigger time" on the other hand, no value is to be determined from the existing diagram because
Here the parameter value C = 100nF has not taken into account - and, incidentally, no resistance value is named,
Which certainly has influence.

The concrete question:
 
Which "minimum retrigger time" applies when using 100nF and 121kOhm?

regards,

kamal
 

  • Hi Kamal,

    The retrigger recovery time isn't related to the external resistor.  It has to do with the time for the internal circuitry of the one-shot to recover from the huge dump of current when a trigger happens, which is only related to the amount of charge the capacitor holds (ie the size of the capacitor).  The datasheet values are correct.  You can retrigger the device after 0.1us regardless of Vcc.If you are operating at 5V, you can retrigger after ~0.05us.

  • Hi,
    Do not understand anymore, If we have 100nF, the retrigger should be more than 1us (figure 7 from datasheet)
  • hi
    I found an other E to E comment :
    As for the retrigger time, this has to do with the discharge rate of the timing circuit. although it is not precise, I would recommend using 0.1*Rext*Cext for this value to be safe. The largest value I have seen in our data is actually 0.09*Rext*Cext. The multiplier decreases inverse to capacitor size -- ie a 1uF capacitor has a multiplier closer to 0.00003, and a 100pF capacitor is closer to 0.09.

    From that I do not understand where this formula coming from?
    does this recommendation (0,1 * Rext * Cext) refer to my actual system (121k / 100nF) which is to be used on our board?
    Is this recommendation based on any technical documentation ????
  • did you – by now - get any official answer to my request, concerning
    the retrigger time (if used 121k/ 100nF) ?
    Can your recommendation (0,1 * R * C – in our case 1,21ms) be officially confirmed (datasheet)?
  • Kamal,

    You are correct - I mistakely read your 100nF as 100pF and gave you the wrong value. The recovery time for 100nF isn't listed on the plot because data was not taken for it. I would estimate it to be ~10us just based on the data available. The best way to verify would be to build your desired circuit and test.

    The answer you saw to Satoshi-san was referenced to some experimental data I took, and looking back at it, I can see that it is incorrect. Rext should not affect the recovery time as previously stated, however the equation I gave would give you a safe time for recovery -- 1.21ms is certainly enough time. I believe that 20 us would be sufficient.

    Can you tell me more about your application? What makes the recovery time so critical? Perhaps we can improve the application rather than going down a rabbit hole on this part.
  • hi,

    So if I understand carefully, the 100nF for the recovery time would give an estimated time of 10us and there is not way to calculated it.

    Can you tell me which equation you gave me ? which is correct.

    I only have the equation you mention :  (0,1 * Rext * Cext) which Rext affect the recovery time.

    so is this equation correct?

    if yes why it is not mention on the datasheet?

    Regarding your question, about the application, I will need to ask the customer but before I need answers from you.

    REGARDS,

    Kamal

     

  •  hi again,

    just to be clear I am only talking about the RETRIGGER time.

    what I need from you is to confirm the equation for the retrigger time : (0.1*Rext*Cext)

    what is the minimum retrigger time possible?

    What is the retrigger time by using 121K and 100nF ?

  • I don't have an equation for the retrigger time of the device - only the information on the datasheet is available.

    I can say that using (0.1*Rext*Cext) will give you a _safe_ retrigger time, however it is MUCH longer than what is necessary for the device. You will be safe retriggering after ~20 us.

  • hi,
    Thank you for your clear message.

    What remains is the feeling that the datasheet lacks important information. Quite
    unusual for TI-devices-datasheets.
  • I can understand your frustration.  

    It is especially difficult in Logic to please everyone with our datasheets since our parts get used in so many varied applications.  In this particular application, a capacitor was chosen outside the values given on the datasheet.  Personally, when I choose external components for an application like this, I try to stick with the ones that the datasheet has already.  If I have to go beyond it, I test them thoroughly myself since the part might have never been designed to work with them.  Fortunately for this case, I have tested this part and found that it is incredibly resilient.  Even with fairly large capacitors (10 uF) it still works perfectly fine.

    I wrote an app note on the subject available here: Designing with the SN74LVC1G123 Monostable Multivibrator

    Unfortunately, I don't think it will help with this particular application.