Other Parts Discussed in Thread: SN74AVC8T245
Hello,
I'm using the SN74AVC4T245 in a SPI circuit on my board and I am seeing an issue where the input voltage at 2A1 is 0V and the output voltage at 2B1 is 0.8V. From the datasheet, it appears that V_OL is around 0.8V at 25mA of current.
Aside from possible board issues of a short or bad solder joint, I was wondering if having the same line (SPI chip select) tied to both OEZ and to one of the input data pins could cause a problem. The below picture shows the schematic. The signal that I'm asking about is labeled SPICSZ0_DLPC.
I hope that my question is clear. Thank you for any assistance!
-Paul