Other Parts Discussed in Thread: EK-TM4C1294XL
I am using TM4c1294EVK board and sending (SPI data line) digital signals CLK, DATA, SYNC to the DAC's. These signals from TI board are routed through interface board to the DAC's in our application board (Unit Under Test - UUT). I would like to drive these signals using 1 mtr cable for testing the UUT which will be kept in environmental chamber. The buffer IC used in the interface board is TXB0108PWR is not capable to drive SPI data over a 1 mtr cable. Can you suggest which TI IC I can use to buffer SPI data over 1 mtr cable length to drive the DAC's ? So that the TXB0108PWR output can be buffered further using small board.
Regards,
Jayasankar
Wipro GE Healthcare
9901400445