I have a customer looking for an 8 bit shift register with an open drain that can support 100mA source current. Vdd is 3.3V. The highest I can find is the SN74LV595A which can handle 50mA.
What can you recommend?
Thanks!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I have a customer looking for an 8 bit shift register with an open drain that can support 100mA source current. Vdd is 3.3V. The highest I can find is the SN74LV595A which can handle 50mA.
What can you recommend?
Thanks!
Look at Power Logic. The TPIC6C595 can handle 100 mA (just barely); the TPIC6B595, 150 mA. And these are 5 V devices.