This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LSF0204: LSF0204 Bandwidth Hz to bps

Part Number: LSF0204
Other Parts Discussed in Thread: TXS0104E,

Hi Sirs,

Sorry to bother you.

We have use TXS0104E before. The data rate are "bps"

24 Mbps (Push Pull) /2 Mbps (Open Drain)

We will use high speed solution LSF0204, we saw the date rate are "Hz"

Supports Up to 100 MHz Up Translation and Greater Than 100 MHz Down Translation at ≤ 30pF Cap Load and Up To 40 MHz Up/Down Translation at 50 pF Cap Load

Is possible to conversion what is LSF0204 max bps?

  • Hello Shu-Cheng,

    Don't worry, it is not a bother. We are happy to answer any questions you may have.

    To convert from frequency to data rate you can simply multiply the frequency by 2. So, 100 MHz would be equivalent to 200 Mbps and 40 MHz would be equivalent to 80 Mbps.