Part Number: TXB0304
Other Parts Discussed in Thread: LSF0204, SN74LVC2T45, SN74LV1T125, SN74AUP1T34
My customer has identified a potential benefit to using, TXB0304, a 4-bit level translator in their new design.
The TXB0304 fits all their desired features, but the power numbers aren't entirely clear to them. In high impedance mode, it says each supply could draw a max of 5uA when in high impedance mode, but doesn't give a typical value for that. Is there anyone who could give more detail about the power consumption of this level translator, or is there another level translator that meets these requirements.
Key features they need:
1) Automatic bi-directional support in push-pull (using for SPI). Alternatively, 2 bits can be locked to one direction, and 2 bits locked to the other.
2) Ability to convert between 1.8V on the low side and anywhere from 2-3V on the high side.
3) Very small (preferably < 2mm x 2mm)
4) Low power when not in use (preferably < 1uA)
Would you please help provide clarification about the power (or tips for how to use it at very low idle power), and any recommendations for other level translators that fit the requirements above?