Part Number: SN74VMEH22501
We are using SN74VMEH22501 buffer in a project of ours
The master of the bus is a CPU board, and in the backplane 6 I/O slots are available, and (in the example below) only two slots are populated with an I/O board
In the CPU board and in each I/O board we have SN74VMEH22501 buffer.
See below the waveform of the signal in input to the SN74VMEH22501 (red) and in output (yellow)
The red signal looks very good to me, instead the signal generated by the buffer shows a lot of ringing.
The signals are terminated with 470R/330R divider
Please can you explain why (and provide suggestion) I see all this ringing?
Is this buffer recommended, too, when we have not so many I/O slots? In figure below it seems like up to 21 slots are used.
We have different backplane configuration: the largest backplane is 6 slot; the shortest has only 1 slot
Thanks in advance
Kind regards
Andrea