I wanted to make sure that it was okay for regular operation to drive a 1.8V input with a 1.5V logic signal. (Vcca = 1.8V, DIR=Vcca for uni-direction translation)
The Vih specification indicates Vcca x 0.65 = 1.17V as the minimum voltage required to ensure a logic HIGH at the output, but I just wanted to confirm that this was a totally acceptable use-case, or if there is any potential odd behaviors if the 1.8V input is driven with a 1.5V logic signal all the time. The inputs to this device are currently mixed between 1.5V and 1.8V, so moving to the lower Vcci "AVC" option would not work, I don't believe. THank you.