Part Number: TXB0104
Hi Team,
my customer used the TXB0104 to convert the SPI 3.3V signals to 5V signal, when no connect to 5V meter device, the TXB0104 output amplitude for clock signal is 0V~5V, however, when they connect the meter device, the output amplitude for clock signal reduced to around 2.5V ~ 5V. Attached are the schematic and the output waveform. Please advise what would be the problem root cuase and how to solve this problem. Thanks.
Regards,
Arthur Huang