Part Number: SN74AC14
Other Parts Discussed in Thread: CD74AC14, SN74ACT14, , LM393
Dears
I want use SN74AC14 or similar CD74AC14 or SN74ACT14 to convert analog signal to digital signal.
To do this, I need to know if they have or not internal clamping diodes t?
If yes, clear, I must use an external in series resistor (i.e. 10k) before input pin to limit the currens
So I can fed a input signal with amplitude more than the +5V (suppose it is my power supply) and obtain the conversion.
I'm sure the 74HC14D have internal clamping diodes but I'm nor sure for these ICs.
I want use AC instead of HC because more performing.
Thanks
Gigi