Other Parts Discussed in Thread: 74ACT16244
Hello,
we have following problem with Hi-Z state of a PWM Trip-Zone:
if PWM output signal is low and Trip-Zone event occurs the output pin remains low. If PWM output state is high and Trip-Zone event occurs the output pin goes from high (3.3V) to approximately 1.7V although we have external pull down resistance of 10kOhm at the output and the internal GPIO pull up resistor is off.
Do you have some ideas what the problem can be or is the Hi-Z state with some internal pullup resistor implemented?
Thank you in advance!
Gennadi