Part Number: SN74LV4T125
Other Parts Discussed in Thread: TXB0104
Hi team,
I have a customer thinking about using the SN74LV4T125, but they have had problems in the past with their input signal not being strong enough to drive input pins enough to make the change.
What is the input current requirement for VI = 0 and VI = 5V when VCC is set to 3.3V? This is to down translate from 5V to 3.3V.
I know that some of the TI buffers have a bus-keeper circuit where the input has to be driven hard enough to switch state from 0 to VCC or VCC to 0. I was wondering if there is such a requirement for this device. My customer rain into this when they used the TXB0104.
Thanks!
Brian