Part Number: LSF0108
Situation:
REF_A= 3.3V;
REF_B = 5V Via 1K resistor to limit current during testing,
EN= +5V via 200K,
Pin 1 = GND,
A pins=open,
B pins +5V via 10k
I am finding that the Ref-A input is acting as a current source when VRef_A - VRef_B > 1.2V. I have replaced the chip, checked the pinout and lifted the Ref_A pin2 to confirm that it is the current source. I would have expected only leakage currents on the ref pins.
Any suggestions?
-CS