1. In the "Recommended Operating Conditions" sections it shows that the range of Vcca and Vccb is 1.65-5.5V but the subsequent specs show ranges, 1.65-1.95V, 2.3-2.7V, 3-3.6V, 4.5-5.5V, which covers most common voltage supply values. My question is can the device be powered by 4.0V and how should the specs be interpreted for a voltage not included in the ranges shown above.
2. How is the total Icc requirement of the device calculated?
3. Is it preferable to have A or B powered from the higher voltage?
4. What value of pull-up resistor should be used for OE* and DIR? It looks like the control inputs leakage current is 2 uA and the driver connected is 10 uA. My calculations indicate that a 10K ohm resistor would work but a value even higher should also work. Any feedback is appreciated especially if I am missing something.
5. Ioh is listed as -24mA for 3V (here again, how would 4V supply affect this value?). What load can this drive to a logic high of 2V (50, 75, 100 ohm)? Figure 2 on page 12 shows Voh vs Ioh and is confusing to me because I don't see the correlation to the device output capability so I must be missing something in my interpretation.