Part Number: TXB0304
Other Parts Discussed in Thread: LSF0204
Hi,
On our previous product, we used the TI TXB0304 to translate from 3.3V to 1.8V on the first pass prototype. We had so much trouble with the part, that we took it off the board for pass B. We are again looking for level translation on our new project. I started looking at other vendors and found a footprint/function compatible part from ON Semi and a functionally equivalent parts from Analog Devices and Maxim. Both vendors specify that their part has a Vl (low side) and a Vcc (high side). The ON device which is pinout compatible has pin 1 as the Vlow side and pin 11 as the Vhigh side. On the TXB0304, pin 1 is Vcca and pin 11 is Vccb. The TI data sheet does not say anywhere that one side should be the low side and implies that the device is ambidextrous. On our last project, we had 3.3V connected to pin 1 and 1.8V connected to pin 11 (which is incorrect on the ON part) and like I said, we did not get it to work. Is it possible that TI has the same restriction (a high side and a low side) and it just isn’t in the spec? We are looking for a translation solution and after our last experience with the TXB0304, we are a bit gun shy.
Thanks,
David