Part Number: SN74LV06A
Hi,
I would like to ask you a max Vol (max low level output) data in case following conditions.
- Vcc = 5.0V
- Iol = 6.25mA(min) to 10mA(max)
Do you have the data of Vol?
Because there are some data under some conditions at datasheet page5, 6.5 section as below.
I suppose the max Vol seems to be lower than 0.55V at Icl=10mA/Vcc=5.0V according to this table.
But if you have more information/data, please let me know.
Thank you for your support.
Best Regards,