Part Number: CD4046B
Hi,
Please tell me how to handle terminals when not using VCO function of CD4046B.
4pin → ?
5pin → ?
6pin → ?
7pin → ?
9pin → ?
10pin → ?
11pin → ?
12pin → ?
best regards
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: CD4046B
Hi,
Please tell me how to handle terminals when not using VCO function of CD4046B.
4pin → ?
5pin → ?
6pin → ?
7pin → ?
9pin → ?
10pin → ?
11pin → ?
12pin → ?
best regards
Pin 4 is an output and can be left open.
Pin 5 is a CMOS input and must have a valid level; set it to logic 1 to disable the VCO.
C1 (at pins 6, 7) must be at least 100 pF (for VDD = 5V); I don't know if this is needed if the VCO does not run.
Pin 9 is an analog input, so I guess you can connect it to any valid voltage level.
Pin 10 is an output and can be left open.
R1 (at pin 11) must be between 5 kΩ and 1 MΩ; I don't know if this is needed if the VCO does not run.
R2 is optional, so pin 12 can be left open.