This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74AUP1G74: SN74AUP1G74 used for frequency divider

Part Number: SN74AUP1G74


Hi, 

we want to use SN74AUP1G74 as frequency 2 divider, generate 48kHz from 96kHz, is it possible? with below connection. 

but i am afraid we may lose the first cycle. 

  • Connecting the inverted output to D indeed creates a frequency divider.

    The initial output state is undefined. However. that logic symbol is incomplete: you can use the P̅R̅E̅ or C̅L̅R̅ inputs to set the state to a defined level at any time.