What pull up resistor should I use on SPI_OE* ? The datasheet makes reference to choosing the resistance value relative to a "driver" but the datasheet is not clear what driver they are talking about.
With a 10kOhm pull up I'm still getting high leakage current from the part when I power off VCCB. Do I also have to pull up or down the A1, A2, A3, A4 and B1, B2, B3, B4 inputs in addition to the SPI_OE* ?