This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LSF0204: LSF0204

Guru 13485 points

Part Number: LSF0204
Other Parts Discussed in Thread: SN74AVC4T774, TXB0104

Loking for similar translator to the LSF0204 but for unidrectional

the current one (bidirectional) makes problems.(it has high output impedance)

  • Hi eli,

    We have many translation solutions available. Can you tell me what you need to translate so I can make a suggestion? Voltage, speed, load conditions, and interface names are all very helpful.
  • Need RUT package and:
    UART : Rx, Tx, CTS, RTS

    MCU : 3.3v BT : 1.8v
    Tx --> Rx
    Rx <-- Tx
    CTS <- RTS
    RTS -> CTS
  • Hello eli,

    I think the SN74AVC4T774 would be a good fit. It has individual direction control pins to configure the lines for your signals and can translate between 3.3V and 1.8V. It is only available in PW, RSV, and RGY packages though.

    The TXB0104 is available in the RUT package and could also work.

    What data rate are you operating at? Are you going to be driving over long traces or cables?